This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are developing a flyback converter with 85-265Vrms 50Hz input to 12V, 1.5A output using the PSR IC UCC27812D. But during our tests we observed that the output is oscillating when a speaker load is used(varying load requirement). Sometimes the VDD drops below UVLO and leads to shut down of the converter. Please find the attached circuit and waveforms for your reference.
Regards,
Akshatha
Input Cap used = 56uF at the rectified input
Hi Akshatha,
Thank you for the query on UCC28712.
I will review the schematic and get back by tomorrow.
Regards,
Harish
Hi Akshatha,
I reviewed the schematic briefly the following are my initial comments:
1/ The Vdd capacitor seems low at 1uF. Try increasing this to 10uF
2. The ouput capacitor at 150uF seems low. Try increasing this to 500-680uF.
3. You could use a CLC type configuration filter at the output. Try putting the heavier capacitors at the output first, then the 10uH inductor and then lower value capacitance like the 22uF whic you have in the schematic.
Please try the above and let us know your feedback.
Regards,
Harish