This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2673: Minimum output current

Part Number: LM2673

If the LM2673 is configured for a max current of 3A (for example) is there any sort of minimum output current that must be maintained?

Input voltage is 24VDC, and the output voltages will be 3.3 VDC to 12VDC (want to use the same part in several different parts of the design)