If several hundred μA of current consumption occurs during sleep mode, will the RM value be updated to reflect this effect?
I feel it would be difficult to do from the followings.
Could you tell me your thought?
V_SR = -0.125 ~ 0.125 V
Resolution = 14 bits
R_SENSE = 10 mohm
Minimum detect current = 0.125 V * 10 mohm / (2^14 / 2) = 1.5 mA/ LSB
I have the issue that after being left for a long time in sleep mode, the battery voltage is low but the RM value is very high.