This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87562-Q1: LP87562PRNFRQ1

Part Number: LP87562-Q1

Hi,

We are using LP87562PRNFRQ1 regulator in our project. May I know after what time the device will shut down after the temperature reaches 130°C and 150°C (Thermal warning and thermal shutdown)? I want to know the same details for TPS62872Y4QWRXSRQ1 at 150°C and 170°C

  • Hi Shishira,

    I do not see this time specifically defined in the datasheet, though there is a deglitch time for each of these defined in Table 7. May I ask why this timing is needed? These are both latching events, so once thermal shutdown temperature is reached (for the period of the deglitch time), the regulators will disable.

    Regards,

    Matt