This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62913: Floating S-CONF pin

Part Number: TPS62913

Hello,

As part of a Failure Modes and Effects Analysis we are performing on a power system based on the TPS62913, we need to consider the possibility of an open circuit on the resistor connected to the S-CONF pin, which will result in the pin being in a floating state. From the datasheet I could not determine whether a default mode or some internal pull-up/down exists on the S-CONF pin.

Could you please inform me if there is a default mode when the S-CONF pin is floating or if the device will start in a random/undefined configuration ?

Thanks in advance !