Other Parts Discussed in Thread: TPS55289, BQ25731
We are considering using the TPS25750 in a sink only application, with 100W (5A 20V) PD.
USB 3.2 only
Battery-less application powered from another USB Sink only port using the TPS25730D
1. Is it possible to use the TPS25750D in a 100W source application (DFP) using the internal power path?
2. is it possible to control the TPS55289 via I2C directly using the TPS55289 with no MCU?
2.1 Do you have any examples?
2.2 If possible can we use the online config. GUI? I cant see any way of doing so, if possible how?
3. Is this the best approach for a USB3.2 100W Source only USB-C port?
Another question for the same product but another application:
4. We have another source only port so above questions remain. But this port will be Displayport only, no USB, so we only need the FLIP function, is it possible to use the TPS25730D in a Displayport Only USB-C source application?