Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hello,
I am trying to run the GPC cycle for the BQ34110 (using the EVM and the EV2400). I have a 12V 6Ah LIFEPO4 battery. I followed the EVM tutorial and using a Digital load at 1.2Amps.
I would like to understand the Cycle setup parameters in BQStudio.
Pre-cycle Discharge End Point (SOC , Voltage)
Discharge End Point (SOC , Voltage)
Question: For those parameters, do I put the termination single cell voltage (=2300mv) or the whole pack termination voltage (4x cells) (=9200mV) ?
When i put the 2300mV cell voltage, i go get an ERROR in the GPC Control log (Start Task Discharge , Unsupported Termination).
If i put the 9200 mV , in the log it says (Start Task: Discharge (Voltage = 9200mV)).
I also have the EDV2 reached showing as green color on the Log (see pic below). Is that OK ?
I followed this excel file provided by Matt Sunna to configure the registers of the BQ34110. Is this OK ?
e2e.ti.com/.../7178.bq34110_5F00_dataflash_5F00_notes_5F00_rev03_5F00_20181002.xlsx
Could you please let me if I am doing the right procedure here ?