This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use TPS6282533DMQ for 5V input and 3.3 V/ 2A output? What would be recommended circuit for this?
Hi Ravi,
Yes you can use TPS6282533DMQ for 5 to 3.3V conversion with 2A load current.
You can use a schematic as below for TPS6282533DMQ as well.
Best regards,
Varun
Hi Ravi,
You can either use 2 capacitors of 10uF or 1 capacitor of 22uF at the output.
Best regards,
Varun