I developed a prototype, related to the datasheet, I measured a very high Vpp ~800mV, what can be wrong ?
I have used the schematic in the datasheet with an inductor from WE 74404084121
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I developed a prototype, related to the datasheet, I measured a very high Vpp ~800mV, what can be wrong ?
I have used the schematic in the datasheet with an inductor from WE 74404084121
Hi Taher,
By reducing your output voltage, you will likely have a larger inductor current ripple, so the output voltage ripple will be increased. You may see this relationship is true with equation 21 in the datasheet.
So a solution is to increase the output capacitance.
Thanks,
Richard
Thank you Richard!
yes, with increasing the caps I could decrease the ripple.
I will do some more tests in the next days