The LM5123-Q1 datasheet says that to use the Programmable Spread Spectrum (Dither) feature connect a capacitor to the SYNC/DITHER/VH/CP pin which then works at about 1V.
The datasheet also says that if you want the charge pump to keep the high-side MOSFET 100% switched on during bypass mode then the SYNC/DITHER/VH/CP pin should be greater than 2.0V
Does this mean that we can not use Programmable Spread Spectrum if we need to run in bypass mode? (Or is there a work-around that allows the SYNC/DITHER/VH/CP pin to switch between the two conditions?)
Best Regards
Chris