This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: Pass-Through behaviour below Vin,min

Part Number: TPS61022


Hi,

I have a question about the Pass-Through behavior of the TPS61022. In my application the TPS61022 will be used to boost 3.3 V to 5 V. During power up of the 3.3 V voltage rail the 5 V output has to stay completely off until the TPS61022 is enabled via it's EN-signal. Is this even possible? Or will the TPS61022 pass through the input voltage if lower than the minimum supply voltage of 0.5 V?

Best regards,

Florian