Other Parts Discussed in Thread: BQ25895
The device fails to charge a flat `liPo battery (flat , 0V as the isolation circuit in battery has isolated the battery as volage is below 3V).
The datasheet says it puts 100mA into a shorted battery - but I findd= that strange as there is no voltage at all present across the battery (should a voltage there even if ther is not battery)
So it charges perfect a batery that hasn't gone into protect mode (aka above 3V) no problem - but doesn't even try when battery has gone to 0V?
Is there a fix ?