Hi,
I am going to use the SPI of BQ7694203 IC and the communications should be done in a 5V level. I am planning to use the REG1 of BQ7694203, for which the datasheet suggests that the REG1 is automatically enabled to 5.5V in the device, which supplies the SPI. Please let me know do I need to connect any external 5V to the REG1 PIN in BQ7694203 or it is truly enabled in the device itself?