I have designed a gate driver card to support a traction inverter which has a rating of (60V rms output, 60A rms output). I have designed a single driver card to support functioning of one single leg/ Half bridge of a 2-level VSI. The IGBT modules used (SKM300GB066D) has a gate charge of 2400nC. According to the design, after connecting an external gate resistance of 1.4 ohms, the peak gate current come to be 6.5A, which is supported by the selected IC. During testing of the inverter. The inverter works fine for 20A rms output currents (with a 1kW small EV motor).
However, when I connect my traction inverter after a step down dc-dc converter ( from 72V battery to 60Vdc), in order to operate an EV induction motor, I see that two of the legs of the inverter are not functional as soon as I turn ON the PWMs of the inverter. The Legs of the inverter that remain unfunctional ( i.e. shows fault at the IC input side) remain the same if I interchange my driver cards. Moreover, when I turn off the mains, and power the PWMs all the driver cards give PWM output. I have tried changing desat resistors (suspecting it draws a huge current during start) to very low values (for tripping at 500A peak), but the result was the same.
Kindly help me out to figure out the issue/cases where ther driver IC would refuse to pass on the PWMs to its secondary side.