Other Parts Discussed in Thread: UCC28950EVM-442, UCC28950, TINA-TI
Hello,
I am working on design of 2.5kW 48V PSFB DC-DC converter using UCC28951 Controller IC. (input voltage: 370 to 410 Vdc)
We tested using on-board UCC28951 IC by following the recommended test procedure given for UCC28950EVM-442 EVM with an electronic load set for 10% loading in CR mode (9.216 ohms).
We provided 400V DC at the Vin terminal and then provided the 12V auxiliary supply to the IC.
But two of the diagonal primary side MOSFETs were blown-off. Also, the input DC power supply ran into OCP protection at 2.75 Amps.
So, could you please suggest the proper testing plan to bring up a PSFB DC-DC converter using UCC28951 IC.
Regards,
Nishant