This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: Gas Gauge parameters updated during relaxation

Part Number: BQ28Z610-R1
Other Parts Discussed in Thread: BQ28Z610

Hello, 

After a charge, the BQ28z610 updated RemainingCapacity, FullChgCap and RSOC for a battery with one cell.

Voltage of the battery = 4.175V after the charge. However, the BQ considers , during the relaxation, 100% RSOC (the reality = 97%).

For information, a GFI was carried out with sucess.

Here, the log file to help understand behaviour:

Chg-08759X-0001-i2c1.csv

Best regards,