This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25155: BQ25155EVM Charging operation

Part Number: BQ25155

Operation has been confirmed using BQ25155EVM.
The app used is "Battery Management Studio".
I would like to perform a charging operation, but the charging current does not flow.
The current flowing to VIN5.0V is 10mA or less.
There is no change even if I set 100mA with ICHG_CTRL 0x13.
Do I need to configure any other settings?
Please professor.