Other Parts Discussed in Thread: TPS1HTC30-Q1, TPS4811-Q1
Hi there,
We currently use your Industrial high-side switch in one of our applications article number TPS27SA08CPWPR.
This switch is designed for 24V usage.
Now we want to build a 48V version of the same product, therefore we are looking for an alternative switch.
The only one I could find so far is the TPS1HTC30-Q1.
This one can handle the necessary 48V but has only a maximum current carrying capacity of 6A.
Unfortunately, that's not enough for us. We are looking for a switch that can deal with up to 10A.
My question is if there is any switch available that is a suitable substitute for either the TPS27SA08CPWPR or the TPS1HTC30-Q1 which can handle the necessary
48V and the maximum current carrying capacity of 10A?
And if there is at the moment nothing available are there any plans to launch such a component?
Thank you and best regards
Patrick