This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: ESD protection BAT and TS pins

Part Number: BQ25798

Hi TI Team, 

Working on a design which will have a removable battery pack. When the Battery pack is removed, the BAT and TS pins will be exposed and susceptible to ESD strikes. 

Researching the TI ESD Essentials videos: Getting started with interface protection | TI.com there are a couple specifications required to select the proper TVS devices:

  • Voltage range
  • Clamp Voltage
  • ESD pulse.

The BAT pin will have a battery 2S battery pack. The working voltage range will be below 9V 

The TS pin Circuit will have a working voltage < 5V.

The ESD pulse target would be IEC61000-4-2 8kv contact/15kv air. (16A)

The TI ESD essentials suggest the clamping voltage should be <= to the TLP (Transient Level Pulse?) 100nS pulse design for the chip.

Can you advise what the TLP specification is for the BAT and TS pins?

Regards,

Jim