This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173: BQ25173 in combination with IRM-01-3.3

Part Number: BQ25173


Hi,

For a design we would like to use the BQ25173 in combination with the IRM-01-3.3 to charge a 3V supercap to 2.7V.

The meanwell power supply has a voltage rating of 3.3 volts with a +/- of 2.5%. This means the power supply would have a minimum low of 3.217V.

The BQ25173 has a VIN_LOWV of maximum 3.15V. That should be enough. But the IRM-01-3.3 also has a maximum ripple and noise rating of 150mVpp. If we take this noise in account we could get under the minimum of 3.15V of the BQ25173.

Could this noise be any problem for the BQ25173?