Other Parts Discussed in Thread: BQ33100, EV2400, BQSTUDIO, BQEVSW
I'm having some issues with how the learning process of BQ33100 works. I have a BQ33100EVM DIV Kit connected to another MCU, and I'm using SMBus. But here's the thing, I can only start the learning process by using the manual learn command. Even though I set the learning frequency to 250, which should be every 10 minutes, it's not happening. And when I do trigger it the manual learn using 0x0023, it starts up, but then it gives me these weird numbers for capacitance and ESR, like 62296 and 32767.
I've 5 supercaps, each 5F 2.7V, all lined up in series, making a total capacitance of 1F, with an ESR of 225mOhm overall. I'm scratching my head wondering what's up with this learning command. Maybe I'm missing something or skipping a step. Any ideas on how to fix this?
Thank you,
Capacitance = 62296 F
Health = 100 %
Current = 500 mA
Operation Status: DSG=0, SS=0, FC=1, LTE=1, CHGOR=0, CB=0, LDTO=0, LCTO=0, LPASS=1, CL=0 , CFET=1
System Voltage = 15235 mV
Design Voltage = 10500 mV
Design Capacitance = 1 F
Init 1st Capacitance = 62296 F
Capacitance = 62296 F
Design ESR = 225 mohm
Initial ESR = 32767 mohm
ESR = 32767 mohm
Learning Frequency (250 is every 10 mins) = 250 weeks
Taper Current = 1
Taper Voltage = 140
Current Taper Window = 5
FC Set = 255
FC Clear = 255
MAC_LIFETIME_AND_CAP_BALANCE = 0 mV
Temperature = 2706 C
0x0A Current 0 mA
0x09 Voltage 10521 V
0x0B ESR 32767 mOhm
0x14 Charging Current = 500 mA
Charging Voltage = 2058 mV
Total Voltage = 10521 mV
Cap 1 Voltage = 2058 mV
Cap 2 Voltage = 2108 mV
Cap 3 Voltage = 2108 mV
Cap 4 Voltage = 2108 mV
Cap 5 Voltage = 2108 mV