This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED Backlight Driver for LCD-TFT Display Panel

Other Parts Discussed in Thread: TPS61195

Hi,

    I need support for a 5.7" LCD backlight.I need two requirements to satisfy.I have to use two Displays and they have different LED backlight config

1.  One is with 3 strings each of 60mA/13.3V

2. The other one with single string 200mA/10V

I need to operate two LCD's from one IC that means i may use any of the LCD in according to availability, and I dont want to design two circuits for it. And I want to operate it from 5Volt supply. So I hope it ll be a boost converter. if could suggest me some SOIC,SSOP packages ,will be nice

Ask me for further clarification.....

Thanks in advance