This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25830A-Q1: bus series resistance function

Part Number: TPS25830A-Q1

Hi team,

Confirm two questions:

1. The resistor on the BUS pin is just for current limiting, right? The manual recommends 100 and the recommended circuit is 10 ohms. How big should I use?

2.What is the electrostatic capability of power paths such as BUS, CSN CSP and other pins? Do I need to add an ESD tube to the power output?