This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317: Constant current drivable LDO

Part Number: LM317
Other Parts Discussed in Thread: BQ25172

Hi,

Is there an LDO like LM317 that can design a constant current circuit for a battery?

The specifications are as follows.

Input voltage: 17V to 19V

Output voltage: 1V to 1.5V

Constant current: 100mA

If possible, three terminals

Best Regards,

Nishie