Other Parts Discussed in Thread: LMR33640
WBDesign_OUT_NEG3p3V_500mA.pdf
Hello,
I have used WEBENCH to generate a -3.3V power supply.
The datasheet of LMZ14201 specifies the minimum voltage 5V.
The topology used is Inverting Buck Boost and might be the reason the generated schematic is correct but I need confirmation for this.
Question: Can LMZ14201 generate -3.3v although in the specs the minimum voltage is 5V (5-0=5 > 0-(-3.3v) = 3.3V)?
Regards,
Marius Raducanu