This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25069: Circuit validation

Part Number: LM25069
Other Parts Discussed in Thread: CSD16415Q5,

Hi team,

We are validating a reference circuit for LM25069PMM-2 that was given to us by a customer.

Under the following conditions.

Could you please tell me if there is a problem with the FET?

I consider the following.
The power rating of the FET is less than 40W, so the power rating needs to be changed.
The SOA margin of the FET is also low, so it is better to replace it with a component with better SOA characteristics.

Design info
=====================================
FET:FDD8896

Input voltage: 12V±5%.

Current Limit: MAX:10A.

Power Limit:64W

Temperature: 25℃ to 60℃.
=====================================
RS=5mΩ

VPWR=75KΩ

CL=1000uF

TIMER=1uF
=====================================

Best regards,