Other Parts Discussed in Thread: TPS922055
Hi Team,
Use TPS922055 driver LED lamp, 36V power, output voltage 20-25V, current 3.5A.
Use the oscilloscope to check the chip 14 pin SW, when the PWM is less than 10%, the output waveform interference is large (PWM is more than 20% waveform is better).
Double-sided circuit board design.
There are two sets of independent output circuits on a circuit board.
36V power waveform also has large interference, how to improve?
The schematic diagram is as follows:

SW waveform diagram is as follows: (@10%PWM)

SW waveform diagram is as follows: (@20%PWM)

36V power waveform diagram is as follows:

Best Regards,
Kevin