Other Parts Discussed in Thread: BQ78350, GPCCEDV
Hi everyone,
we have a bq78350r1 on a 7S4P pack. We successfully created a CEDV GI in a temperature range of -20°C-+40°C. So lowtemp = -20°C; roomtemp = 0°C; hightemp = 40°C, because this is the temperature range the battery pack will be in use.
We got good results from the GPC Packager tool and all the deviations were within recomended range. However, when we did one charge/discharge cycle we could see the battery pack could only learn around 11.900mAh and not the designed 12.800mAh.
So my question is is the temperature range of the CEDV log files too high? Our approach would be to skip the -20°C and start two more measurements with roomtemp = 20°C and set lowtemp = 0°C and say that the design capacity is reachable in "normal" temperature range but whenever it gets colder there could be some losses in capacity.
Any help is appreciated!
GI_v06.gg.csv3343.lowtemp_highrate.csv3343.lowtemp_lowrate.csv7167.roomtemp_lowrate.csv7167.hightemp_lowrate.csv1781.hightemp_highrate.csv1781.roomtemp_highrate.csv 1781.GPCPackaged.zip