Other Parts Discussed in Thread: TPS2597, TPS25981, TPS2595
Hi team,
do we have a recommendation for below request?
1. When used on a 12V power supply, the upper limit of the input voltage of the IC needs to support 18V (just a little higher than 18V, and the package will be very large if it is higher), and there is no requirement for the lower limit (below 10V);
2. The package should be as small as possible, preferably integrated Power FET, and the fewer peripheral circuits, the better;
3. The current limit is adjustable, and the Current Limit needs to be greater than 2A;