This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS922054: Fast Trigger for LED Flash without wakeup delay

Part Number: TPS922054

I need a fast reaction for a LED flash for industrial vision application and need some help.

The TPS922054 seems to be great but I see one issue.

If this Driver is longer then 57ms not enable (PWM input minimum off time to disable device)  it needs longer wakeup routine from about 300us.

I need a direct output current after I enable the Driver (max 2us delay).

is there any way how to avoid this wakeup time? Or is it necessary to send a short pulse every 50ms to keep the driver awake?

Thanks for your support!