Other Parts Discussed in Thread: BQSTUDIO
Hello folks ,
BQ76952 : I want to use alert pin as ALERT SIGNAL when any fault is triggered except CUV.
I have configured setting:AlertPinConfig, Setting: Default Alarm Mask , SF Alert mask A but still We have facing some issue.
Please find configuration as below
Alert pin config : 0x22 (the output voltage is driven by the REG1 LDO (which can be programmed from 1.8 V to 5.0 V))
Default Alarm mask : 0X1000 (As want decision based on SF Alert mask register)
SF Alert mask A : 0XF8 (Disable CUV Bit for Alert pin)
Issue : When i checked alert pin signal for CUV fault alert pin is not getting high as per expected behaviour as disabled in SF Alert A register , but when any other fault along with CUV triggred for example UTC in that case Alert pin change its state to high(Which is expected) but UTC fault is solved and CUV fault is present at that time ALERT Signal is high for CUV also which is disable. Can you please help me with this issue. ?AfterDefaultAlarmMaskChange.gg.csv