Hi there,
I have an issue with the TLVM13640RDLR trying to generate a 5 V output from a 24 V input at VIN. The circuit has a USB-OTG port for standard communication and first programming of a processor module from within a pc. The design works fine in usual use-case.
Whenever a connect the USB cable prior to connecting the power supply (24 V at VIN) the IC an unusual behaviour of the circuit happens. The 5 V rail is not stable anymore!
Page 18 on the datasheet states: "The VLDOIN voltage must not exceed both VIN and 12 V."
Due to the connection of USB => VOUT1, VOUT2 and VLDOIN (shorted to VOUT1 and VOUT2 on the circuit) gets 5 V from USB (VBUS). VIN is still not active. This leads to VLDOIN > VIN (= 0V).
Does this harm the IC? Is there a work around to avoid this problem?
schematic of "TLVM13640" along with the used power switch (TPS2560DRCT) towards the USB connector. VBUS is acutally needed by the module for detection purposes...

Best
Lait