Other Parts Discussed in Thread: TPS25750, TPS25751
Hello,
I have a question related to the compatibility between the BQ25756 battery charger and the TPS25750 PD controller. With the information obtained from another thread (https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1294407/bq25756-bq25756/4931274?tisearch=e2e-sitesearch&keymatch=%25252520user%2525253A582581#4931274), I know that the TPS25750 is compatible with the BQ25756 and the TPS25751 is compatible pin to pin with the TPS25750, so the TPS25751 can be a direct replacement of the TPS25750.
But now I am wondering if the firmware generated (in the application customization tool) for the TPS25751, with the BQ25756 integrated, can also been applied to the TPS25750 or it need a reconfiguration or adaptation because any difference between the TPS25750 and the TPS25751.
I say that because in the application customization tool applied to the TPS25750, the battery charger BQ25756 doesn't appear and I don't know how to generate the firmware to the TPS25750 to be associated with BQ25756.
In summary:
1.- Is there any way to generate the firmware for the TPS25750 with the BQ25756 integrated?
2.- Can I generate the firmware for the TPS25751 with the BQ25756 integrated and then flash it on the TPS25750 with the BQ25756 integrated?
3.- What are the main differences between the TPS25750 and the TPS25751?
Best regards,
Jose Jiménez