Other Parts Discussed in Thread: TPS2662
Customer is doing the STO circuit with TPS26600PWPR for Robotics application. Few questions are here.
- Is enable function able to be implemented on UVLO pin of TPS2662?
Below is test on bench, the voltage on the UVLO pin needs to be higher than 1.175 to 1.225V to turn on the switch. Is this circuitry correct?
- What's the different between the V_UVLOR defined on the section 7.5 and 7.7.
As i understand here:
On 7.5, it is device to device variation over temp
On 7.7, It should be UVLO threshold vs. temp. it should be tested with the same device.