Other Parts Discussed in Thread: TPS51386
Hi,
I want know which is the correct value while selecting the output inductor value for 3.3V/8A Output.
Design Input:
VinMin = 10V
Vin Max = 16V
Vin Typ = 12V
Vout = 3.3V /A
Mode = Eco
Soft start = default ( 1.3mS)
According to the datasheet the Output inductor value for 3.3V - ECo mode as below:

But while using the Webench, The output Inductor value is 2.2uH.
The webench simulation attached here for your reference.
Please clarify which is correct.
Best Regards,
Mohamed.3.3V@8A-TPS51396A.pdf