This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61495-Q1: Definition of I_RATED in equations

Part Number: LM61495-Q1
Other Parts Discussed in Thread: LM61495

Looking through the datasheet, I see a couple references to I_RATED:

  (equation 6)

 (equation 4)

Is I_RATED referring to the DC max current rating of my selected inductor or of the model of LM61495 itself (6, 8, or 10A)?

Thanks!