Hi,
Please answer our customer's questions.
1. Whether PWMx is processed when OUTPUT DIMMING (PWM) is not used
- Do I have to use it above PWMx threshold voltage? Can I connect to Floating or GND?
2. Integrated output 4CH for 1 OUTPUT
- Can I use only 1 R_RESx & C_OUTx?
- Can't I use only one R_SNSx?
3. Whether some output CH is processed when not in use
- RESx 및 OUTx : Floating
- INx : VCC+
- PWMx : GND
4. Should I connect to GND if FAULT is not in use?