This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV103: Duty cycle of PWM Signal not accurate as per datasheet declared resistor value

Part Number: DRV103


Hi Team,

Good Day...

This is Kirubakar Nagarajan from Rotork Controls Limited. I have implemented DRV103H IC for solenoid driving with 50% duty cycle. I have used 215K resistor for setting IC oscillator frequency @ 24KHz and 137K Resistor implemented to have 50% duty cycle of PWM signal output from DRV IC. All resistor tolerance are selected with 1% limit and when I captured the signal in DSO, the duty cycle is not 50%. Could you please clarify the issue.

I have attached  the waveform for your reference.