Other Parts Discussed in Thread: TPS3760, TPS3762
I'm searching for an IC from TI that provides the AC line brown out protection feature. The device will be used as a supervisory IC to rise a reset signal that will be used to disable an AC to DC power System when the AC line is below typ 190Vac and allow auto restart when the input voltage is above the startup threshold typ 208Vac.
I'm considering using the TLV840 Nano-Power Ultra-Low Voltage Supervisor IC after the Single-Phase Diode Bridge Rectifier. It will provide an adjustable reset time delay ranging from 50msec to 200msec. However, I'm investigating if there is a better suitable component available from TI.
Kind regards.