This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ75614-Q1: Use of external clamp diodes

Part Number: BQ75614-Q1

Hello TI team,

For BQ75614-Q1, to protect the device against high voltage (<60V) short on the CB lines, do you recommend to use external diodes?

If there is any application report on this topic, kindly share.

If the external resistors are limiting the current below <200mA, and if this current flows through body diode of internal balancing FETs due to short to other high voltage line, is there any concern?

can you specify body diode current limit?

Thank you!