Hi,
I am little bit confused about OVER DISCHARGE CURRENT and SHORT CIRCUIT detection .
As mentioned in the datasheet OCD and SCD is detected based on V- to VSS voltage , where SCD will consider the hike in 10us .
in my circuit when the OCD is triggered as told the Dout goes low but it will not retain when i decrease the load Current why is it like that ?
and in SCD when the short is released it will retain the normal state, since both are depend on the V- to VSS voltage , is it proper ?
can you briefly explain the difference between OCD and SCD .
Regards ,
SANATH KUMAR