Part Number: USB-C-PD-DUO-EVM
Hello,
I'm trying to use the USB-C-PD-DUO-EVM by following the USB-C-PD-DUO-EVM User's Guide,
but I'm noticing that there are differences between the SW release date
"
TPS65981_2_7_8 Application Customization Tool
GUI Version: 6.1.4
Release date: March 29, 2023
"
and the date of the manual
"SLVUBJ5–October 2018".
Q1 - Would it be possible to have a version of the manual aligned with the SW release date?
In any case I'm trying to take the first steps, but I'm having a lot of problems.
My HW is this: J1 powered with 19,5V, PC connected with a usb micro cable to the EVM.
As for the interface connection, I believe this is there, in fact with the usb micro disconnected
I get this message
"Exception Encountered during FTDI Adapter Selection:No FTDI I2C channels (I2C_GetNumChannels) detected, exiting....
<type 'exceptions.Exception'>
"
while when the micro usb cable is connected I get this popup when I click on "adapter"

but if I perform the Sweep I2C Addresses it fails

then if I try "TEST I2C HI READ (MODE REGISTER 0x03)
I get this FAIL MESSAGE
then if I try "TEST I2C HI READ (MODE REGISTER 0x0F)
I get this FAIL MESSAGE
then if I try "TEST SPI FLASH READ (Address 0x00)
I get this SUCCESS MESSAGE
Q2 - how can I fix the problem (if any) with I2C?
Q3 - which is the file to be loaded, that I cannot find source.bin or sink.bin?
Q4 - when loaded a .bin file wuth "change file" button, which is the command to start flash?
Thanks
Alessandro