Hi,
Can I use BQ25898 for charging a parallel 2 cell as below shown.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sreejitha,
Yes the BQ25898 device can be used to charge 2 cells in parallel.
Best Regards,
Garrett
Hi Garnett,
We are planning to use such a battery charger for secondary charging option for our device. Primary charging is with a dedicated PMIC with USB charging.
So we are in search for a charger IC without the following pins. Kindly let us know whether TI has any solution for our requirement.
Following pins not required.
Hi Sreejitha,
What is your requirement for charge current on the secondary charger? Do you have a package preference (WCSP verse QFN)? If you are specifically looking for a buck converter charger some of the pins you mention as unneeded are on every option TI has to offer.
For example, TS pin for battery temperature monitoring is on every battery charger we have. If you do not wish to use this function TS pin can be connected between two 10kohm resistors from REGN pin to GND.
Similarly, the ILIM pin for setting input current limit is on the vast majority of our charger options. Please be aware there is a register bit (REG00 bit 6 'EN_ILIM') on BQ25898 which can be set to disable ILIM pin. With EN_ILIM = 0 ILIM pin can be left floating.
The other pins you mention can simply be connected to GND or left floating. Please see my comments on each specific pin below.
Best Regards,
Garrett
Hi Garnett,
Thank you for the suggestions.
Kindly have a look into the schematics and share your valuable feedback.

Hi Sreejitha,
Please see my comments below.
All other connections shown look good to me.
Best Regards,
Garrett