This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: register write time

Part Number: TPS6594-Q1
Other Parts Discussed in Thread: LP8764-Q1

Dear expert,

Customer write tps6594-Q1 and LP8764-Q1 register and then read back to check.

How much delay they need to wait before check? Is there any special register they need to wait longer?

Thanks

  • Hello Ryan,

    How much delay they need to wait before check?

    There's no specified readback time wait, 100kHz or 400kHz clock there have been no issues.

    Is there any special register they need to wait longer?

    There are many special functions which require wait times when trying to communicate with the PMIC:

    • RUNTIME_BIST -> 3.5ms
    • EN_CRC -> 3ms
    • nRSTOUT -> Resets the I2C controller on the device when toggled

    BR,

    Nicholas