Part Number: BQ24196
Other Parts Discussed in Thread: TUSB320, BQ24195, BQ24190, BQ25890H, BQ25611D
Hi
The customer designs a control board with battery and OTG functions and wants to use the following chips to implement OTG and charging
BQ24196--charging IC
TUSB320--cc logic chip, configured in DRP mode, ID is connected to the OTG pin of BQ24196 through pull-up
They want to use D+ and D- to detect the actual output current limit through the BC1.2 of the charger protocol, but D+ and D- are occupied by the microcontroller, and this microcontroller does not support the detection of the above protocol.
Currently, the input current is only detected through the cc logic of the TUSB320. However, since most chargers only have a type-A interface, and the connecting line only has a 56k pull-up resistor, it is impossible to use CC to determine whether it can support the output of 2A current. (It is impossible to identify which is a host such as a computer host and which is the host and which is the adapter when using the A to C line.)