Hi team:
My customer target to use LM5177 for IND power module:
DC: 9~60Vin, 0~60Vout, with 20A at 1200W. May need two modules connected in parallel and each module outputs 600W.
base on the buck - boost model as above. The duty cycle of the G1 will affect the inductor peak current, We currently selecting an inductor, but I don’t know the duty cycle of the S1.
and customer will have external input current limiter circuit, so the actually production do not need high peak current `s inductor. would you help to share the relationship formula between Duty1, Duty4 and input and output?
tks again.