This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: BQ27441EVM-G1A: Failed to read battery capacity

Part Number: BQ27441-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi

BQ27441 1-0055: rom_mode_gauge_dm_init: INITCOMP not set after 100 seconds

/*
 * BQ27x00 battery driver
 *
 * Copyright (C) 2008 Rodolfo Giometti <giometti@linux.it>
 * Copyright (C) 2008 Eurotech S.p.A. <info@eurotech.it>
 * Copyright (C) 2010-2011 Lars-Peter Clausen <lars@metafoo.de>
 * Copyright (C) 2011 Pali Rohár <pali.rohar@gmail.com>
 *
 * Based on a previous work by Copyright (C) 2008 Texas Instruments, Inc.
 *
 * This package is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 *
 * THIS PACKAGE IS PROVIDED ``AS IS'' AND WITHOUT ANY EXPRESS OR
 * IMPLIED WARRANTIES, INCLUDING, WITHOUT LIMITATION, THE IMPLIED
 * WARRANTIES OF MERCHANTIBILITY AND FITNESS FOR A PARTICULAR PURPOSE.
 *
 */

/*
 * Datasheets:
 * http://focus.ti.com/docs/prod/folders/print/bq27000.html
 * http://focus.ti.com/docs/prod/folders/print/bq27500.html
 * http://www.ti.com/product/bq27411-g1
 * http://www.ti.com/product/bq27421-g1
 * http://www.ti.com/product/bq27425-g1
 * http://www.ti.com/product/bq27441-g1
 */

#include <linux/module.h>
#include <linux/param.h>
#include <linux/jiffies.h>
#include <linux/workqueue.h>
#include <linux/delay.h>
#include <linux/platform_device.h>
#include <linux/power_supply.h>
#include <linux/idr.h>
#include <linux/i2c.h>
#include <linux/slab.h>
#include <asm/unaligned.h>
#include <linux/gpio.h>

#include <linux/power/bq27441_battery.h>

#define DRIVER_VERSION			"1.2.0"

#define INVALID_REG_ADDR		0xFF

//#define CHARGE_EN 94

int g_capacity;

enum bq27xxx_reg_index {
	BQ27XXX_REG_CTRL = 0,
	BQ27XXX_REG_TEMP,
	BQ27XXX_REG_INT_TEMP,
	BQ27XXX_REG_VOLT,
	BQ27XXX_REG_AI,
	BQ27XXX_REG_FLAGS,
	BQ27XXX_REG_TTE,
	BQ27XXX_REG_TTF,
	BQ27XXX_REG_TTES,
	BQ27XXX_REG_TTECP,
	BQ27XXX_REG_NAC,
	BQ27XXX_REG_FCC,
	BQ27XXX_REG_CYCT,
	BQ27XXX_REG_AE,
	BQ27XXX_REG_SOC,
	BQ27XXX_REG_DCAP,
	BQ27XXX_POWER_AVG,
	NUM_REGS
};

/* bq27500 registers */
static __initdata u8 bq27500_regs[NUM_REGS] = {
	0x00,	/* CONTROL	*/
	0x06,	/* TEMP		*/
	0xFF,	/* INT TEMP -NA	*/
	0x08,	/* VOLT		*/
	0x14,	/* AVG CURR	*/
	0x0A,	/* FLAGS	*/
	0x16,	/* TTE		*/
	0x18,	/* TTF		*/
	0x1c,	/* TTES		*/
	0x26,	/* TTECP	*/
	0x0C,	/* NAC		*/
	0x12,	/* LMD(FCC)	*/
	0x2A,	/* CYCT		*/
	0x22,	/* AE		*/
	0x2C,	/* SOC(RSOC)	*/
	0x3C,	/* DCAP(ILMD)	*/
	0x24,	/* AP		*/
};

/* bq27520 registers */
static __initdata u8 bq27520_regs[] = {
	0x00,	/* CONTROL	*/
	0x06,	/* TEMP		*/
	0xFF,	/* INT TEMP - NA*/
	0x08,	/* VOLT		*/
	0x14,	/* AVG CURR	*/
	0x0A,	/* FLAGS	*/
	0x16,	/* TTE		*/
	0x18,	/* TTF		*/
	0x1c,	/* TTES		*/
	0x26,	/* TTECP	*/
	0x0C,	/* NAC		*/
	0x12,	/* LMD		*/
	0xFF,	/* CYCT - NA	*/
	0x22,	/* AE		*/
	0x2C,	/* SOC(RSOC	*/
	0xFF,	/* DCAP(ILMD) - NA */
	0x24,	/* AP		*/
};

/* bq2753x registers */
static __initdata u8 bq2753x_regs[] = {
	0x00,	/* CONTROL	*/
	0x06,	/* TEMP		*/
	0xFF,	/* INT TEMP - NA*/
	0x08,	/* VOLT		*/
	0x14,	/* AVG CURR	*/
	0x0A,	/* FLAGS	*/
	0x16,	/* TTE		*/
	0xFF,	/* TTF - NA	*/
	0xFF,	/* TTES - NA	*/
	0xFF,	/* TTECP - NA	*/
	0x0C,	/* NAC		*/
	0x12,	/* LMD(FCC)	*/
	0x2A,	/* CYCT		*/
	0xFF,	/* AE - NA	*/
	0x2C,	/* SOC(RSOC)	*/
	0xFF,	/* DCAP(ILMD) - NA */
	0x24,	/* AP		*/
};

/* bq27200 registers */
static __initdata u8 bq27200_regs[NUM_REGS] = {
	0x00,	/* CONTROL	*/
	0x06,	/* TEMP		*/
	0xFF,	/* INT TEMP - NA	*/
	0x08,	/* VOLT		*/
	0x14,	/* AVG CURR	*/
	0x0A,	/* FLAGS	*/
	0x16,	/* TTE		*/
	0x18,	/* TTF		*/
	0x1c,	/* TTES		*/
	0x26,	/* TTECP	*/
	0x0C,	/* NAC		*/
	0x12,	/* LMD(FCC)	*/
	0x2A,	/* CYCT		*/
	0x22,	/* AE		*/
	0x0B,	/* SOC(RSOC)	*/
	0x76,	/* DCAP(ILMD)	*/
	0x24,	/* AP		*/
};

/* bq274xx registers */
static __initdata u8 bq27441_regs[NUM_REGS] = {
	0x00,	/* CONTROL	*/
	0x02,	/* TEMP		*/
	0x1e,	/* INT TEMP	*/
	0x04,	/* VOLT		*/
	0x10,	/* AVG CURR	*/
	0x06,	/* FLAGS	*/
	0xFF,	/* TTE - NA	*/
	0xFF,	/* TTF - NA	*/
	0xFF,	/* TTES - NA	*/
	0xFF,	/* TTECP - NA	*/
	0x08,	/* NAC		*/
	0x0E,	/* FCC		*/
	0xFF,	/* CYCT - NA	*/
	0xFF,	/* AE - NA	*/
	0x1C,	/* SOC		*/
	0x3C,	/* DCAP - NA	*/
	0x18,	/* AP		*/
};

/* bq276xx registers - same as bq274xx except CYCT */
static __initdata u8 bq276xx_regs[NUM_REGS] = {
	0x00,	/* CONTROL	*/
	0x02,	/* TEMP		*/
	0x1e,	/* INT TEMP	*/
	0x04,	/* VOLT		*/
	0x10,	/* AVG CURR	*/
	0x06,	/* FLAGS	*/
	0xFF,	/* TTE - NA	*/
	0xFF,	/* TTF - NA	*/
	0xFF,	/* TTES - NA	*/
	0xFF,	/* TTECP - NA	*/
	0x08,	/* NAC		*/
	0x0E,	/* FCC		*/
	0x22,	/* CYCT		*/
	0xFF,	/* AE - NA	*/
	0x1C,	/* SOC		*/
	0x3C,	/* DCAP - NA	*/
	0x18,	/* AP		*/
};

/*
 * SBS Commands for DF access - these are pretty standard
 * So, no need to go in the command array
 */
#define BLOCK_DATA_CLASS		0x3E
#define DATA_BLOCK			0x3F
#define BLOCK_DATA			0x40
#define BLOCK_DATA_CHECKSUM		0x60
#define BLOCK_DATA_CONTROL		0x61

/* bq274xx/bq276xx specific command information */
#define BQ27441_UNSEAL_KEY		0x80008000
#define BQ27441_SOFT_RESET		0x43

#define BQ27441_FLAG_ITPOR				0x20
#define BQ27441_CTRL_STATUS_INITCOMP	0x80

#define BQ27XXX_FLAG_DSC		BIT(0)
#define BQ27XXX_FLAG_SOCF		BIT(1) /* State-of-Charge threshold final */
#define BQ27XXX_FLAG_SOC1		BIT(2) /* State-of-Charge threshold 1 */
#define BQ27XXX_FLAG_FC			BIT(9)
#define BQ27XXX_FLAG_OTD		BIT(14)
#define BQ27XXX_FLAG_OTC		BIT(15)

/* BQ27000 has different layout for Flags register */
#define BQ27200_FLAG_EDVF		BIT(0) /* Final End-of-Discharge-Voltage flag */
#define BQ27200_FLAG_EDV1		BIT(1) /* First End-of-Discharge-Voltage flag */
#define BQ27200_FLAG_CI			BIT(4) /* Capacity Inaccurate flag */
#define BQ27200_FLAG_FC			BIT(5)
#define BQ27200_FLAG_CHGS		BIT(7) /* Charge state flag */

#define BQ27200_RS			20 /* Resistor sense */
#define BQ27200_POWER_CONSTANT		(256 * 29200 / 1000)

/* Subcommands of Control() */
#define CONTROL_STATUS_SUBCMD		0x0000
#define DEV_TYPE_SUBCMD			0x0001
#define FW_VER_SUBCMD			0x0002
#define DF_VER_SUBCMD			0x001F
#define RESET_SUBCMD			0x0041
#define SET_CFGUPDATE_SUBCMD		0x0013
#define SEAL_SUBCMD			0x0020

/* Location of SEAL enable bit in bq276xx DM */
#define BQ276XX_OP_CFG_B_SUBCLASS	64
#define BQ276XX_OP_CFG_B_OFFSET		2
#define BQ276XX_OP_CFG_B_DEF_SEAL_BIT	(1 << 5)

struct bq27x00_device_info;
struct bq27x00_access_methods {
	int (*read)(struct bq27x00_device_info *di, u8 reg, bool single);
	int (*write)(struct bq27x00_device_info *di, u8 reg, int value,
			bool single);
	int (*blk_read)(struct bq27x00_device_info *di, u8 reg, u8 *data,
		u8 sz);
	int (*blk_write)(struct bq27x00_device_info *di, u8 reg, u8 *data,
		u8 sz);
};

enum bq27x00_chip { BQ27200, BQ27500, BQ27520, BQ27441, BQ276XX, BQ2753X};

struct bq27x00_reg_cache {
	int temperature;
	int time_to_empty;
	int time_to_empty_avg;
	int time_to_full;
	int charge_full;
	int cycle_count;
	int capacity;
	int energy;
	int flags;
	int power_avg;
	int health;
};

struct dm_reg {
	u8 subclass;
	u8 offset;
	u8 len;
	u32 data;
};

struct bq27x00_device_info {
	struct device 		*dev;
	int			id;
	enum bq27x00_chip	chip;

	struct bq27x00_reg_cache cache;
	int charge_design_full;

	unsigned long last_update;
	struct delayed_work work;

	struct power_supply	bat;

	struct bq27x00_access_methods bus;

	struct mutex lock;

	int fw_ver;
	int df_ver;
	u8 regs[NUM_REGS];
	struct dm_reg *dm_regs;
	u16 dm_regs_count;
};

static __initdata enum power_supply_property bq27x00_battery_props[] = {
	POWER_SUPPLY_PROP_STATUS,
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	POWER_SUPPLY_PROP_TIME_TO_EMPTY_NOW,
	POWER_SUPPLY_PROP_TIME_TO_EMPTY_AVG,
	POWER_SUPPLY_PROP_TIME_TO_FULL_NOW,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_CHARGE_NOW,
	POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN,
	POWER_SUPPLY_PROP_CYCLE_COUNT,
	POWER_SUPPLY_PROP_ENERGY_NOW,
	POWER_SUPPLY_PROP_POWER_AVG,
	POWER_SUPPLY_PROP_HEALTH,
};

static __initdata enum power_supply_property bq27520_battery_props[] = {
	POWER_SUPPLY_PROP_STATUS,
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	POWER_SUPPLY_PROP_TIME_TO_EMPTY_NOW,
	POWER_SUPPLY_PROP_TIME_TO_EMPTY_AVG,
	POWER_SUPPLY_PROP_TIME_TO_FULL_NOW,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_CHARGE_NOW,
	POWER_SUPPLY_PROP_ENERGY_NOW,
	POWER_SUPPLY_PROP_POWER_AVG,
	POWER_SUPPLY_PROP_HEALTH,
};

static __initdata enum power_supply_property bq2753x_battery_props[] = {
	POWER_SUPPLY_PROP_STATUS,
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	POWER_SUPPLY_PROP_TIME_TO_EMPTY_NOW,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_CHARGE_NOW,
	POWER_SUPPLY_PROP_POWER_AVG,
	POWER_SUPPLY_PROP_HEALTH,
	POWER_SUPPLY_PROP_CYCLE_COUNT,
};

static __initdata enum power_supply_property bq27441_battery_props[] = {
//added by yue.zhong at 2017-05-08 14:40
//	POWER_SUPPLY_PROP_STATUS,
//end added by yue.zhong at 2017-05-08 14:40
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_CHARGE_NOW,
	POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN,
	POWER_SUPPLY_PROP_HEALTH,
};

static __initdata enum power_supply_property bq276xx_battery_props[] = {
	POWER_SUPPLY_PROP_STATUS,
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_CHARGE_NOW,
	POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN,
	POWER_SUPPLY_PROP_CYCLE_COUNT,
};

/*
 * Ordering the parameters based on subclass and then offset will help in
 * having fewer flash writes while updating.
 * Customize these values and, if necessary, add more based on system needs.
 */
static struct dm_reg bq27441_dm_regs[] = {
	{82, 0, 2, 15729},	/* Qmax */
	{82, 5, 1, 0x81},	/* Load Select */
	{82, 10, 2, 4000},	/* Design Capacity */
	{82, 12, 2, 15200},	/* Design Energy */
	{82, 16, 2, 3000},	/* Terminate Voltage */
	{82, 27, 2, 110},	/* Taper rate */
};

static struct dm_reg bq276xx_dm_regs[] = {
	{64, 2, 1, 0x2C},	/* Op Config B */
	{82, 0, 2, 1000},	/* Qmax */
	{82, 2, 1, 0x81},	/* Load Select */
	{82, 3, 2, 1340},	/* Design Capacity */
	{82, 5, 2, 3700},	/* Design Energy */
	{82, 9, 2, 3250},	/* Terminate Voltage */
	{82, 20, 2, 110},	/* Taper rate */
};

static unsigned int por_detect_flag = 0;
static unsigned int poll_interval = 360;
module_param(poll_interval, uint, 0644);
MODULE_PARM_DESC(poll_interval, "battery poll interval in seconds - " \
				"0 disables polling");

/*
 * Forward Declarations
 */
static int read_dm_block(struct bq27x00_device_info *di, u8 subclass,
	u8 offset, u8 *data);


/*
 * Common code for BQ27x00 devices
 */

static inline int bq27xxx_read(struct bq27x00_device_info *di, int reg_index,
		bool single)
{
	int val;

	/* Reports 0 for invalid/missing registers */
	if (!di || di->regs[reg_index] == INVALID_REG_ADDR)
		return 0;

	val = di->bus.read(di, di->regs[reg_index], single);

	return val;
}

static inline int bq27xxx_write(struct bq27x00_device_info *di, int reg_index,
		int value, bool single)
{
	if (!di || di->regs[reg_index] == INVALID_REG_ADDR)
		return -1;

	return di->bus.write(di, di->regs[reg_index], value, single);
}

static int control_cmd_wr(struct bq27x00_device_info *di, u16 cmd)
{
	dev_dbg(di->dev, "%s: cmd - %04x\n", __func__, cmd);

	return di->bus.write(di, BQ27XXX_REG_CTRL, cmd, false);
}

static int control_cmd_read(struct bq27x00_device_info *di, u16 cmd)
{
	dev_dbg(di->dev, "%s: cmd - %04x\n", __func__, cmd);

	di->bus.write(di, BQ27XXX_REG_CTRL, cmd, false);

	msleep(5);

	return di->bus.read(di, BQ27XXX_REG_CTRL, false);
}
/*
 * It is assumed that the gauge is in unsealed mode when this function
 * is called
 */
static int bq276xx_seal_enabled(struct bq27x00_device_info *di)
{
	u8 buf[32];
	u8 op_cfg_b;

	if (!read_dm_block(di, BQ276XX_OP_CFG_B_SUBCLASS,
		BQ276XX_OP_CFG_B_OFFSET, buf)) {
		return 1; /* Err on the side of caution and try to seal */
	}

	op_cfg_b = buf[BQ276XX_OP_CFG_B_OFFSET & 0x1F];

	if (op_cfg_b & BQ276XX_OP_CFG_B_DEF_SEAL_BIT)
		return 1;

	return 0;
}

#define SEAL_UNSEAL_POLLING_RETRY_LIMIT	1000

static inline int sealed(struct bq27x00_device_info *di)
{
	return control_cmd_read(di, CONTROL_STATUS_SUBCMD) & (1 << 13);
}

static int unseal(struct bq27x00_device_info *di, u32 key)
{
	int i = 0;

	dev_dbg(di->dev, "%s: key - %08x\n", __func__, key);

	if (!sealed(di))
		goto out;

	di->bus.write(di, BQ27XXX_REG_CTRL, key & 0xFFFF, false);
	msleep(5);
	di->bus.write(di, BQ27XXX_REG_CTRL, (key & 0xFFFF0000) >> 16, false);
	msleep(5);

	while (i < SEAL_UNSEAL_POLLING_RETRY_LIMIT) {
		i++;
		if (!sealed(di))
			break;
		msleep(10);
	}

out:
	if (i == SEAL_UNSEAL_POLLING_RETRY_LIMIT) {
		dev_err(di->dev, "%s: failed\n", __func__);
		return 0;
	} else {
		return 1;
	}
}

static int seal(struct bq27x00_device_info *di)
{
	int i = 0;
	int is_sealed;

	dev_dbg(di->dev, "%s:\n", __func__);

	is_sealed = sealed(di);
	if (is_sealed)
		return is_sealed;

	if (di->chip == BQ276XX && !bq276xx_seal_enabled(di)) {
		dev_dbg(di->dev, "%s: sealing is not enabled\n", __func__);
		return is_sealed;
	}

	di->bus.write(di, BQ27XXX_REG_CTRL, SEAL_SUBCMD, false);

	while (i < SEAL_UNSEAL_POLLING_RETRY_LIMIT) {
		i++;
		is_sealed = sealed(di);
		if (is_sealed)
			break;
		msleep(10);
	}

	if (!is_sealed)
		dev_err(di->dev, "%s: failed\n", __func__);

	return is_sealed;
}

#define CFG_UPDATE_POLLING_RETRY_LIMIT 50
static int enter_cfg_update_mode(struct bq27x00_device_info *di)
{
	int i = 0;
	u16 flags;

	dev_dbg(di->dev, "%s:\n", __func__);

	if (!unseal(di, BQ27441_UNSEAL_KEY))
		return 0;

	control_cmd_wr(di, SET_CFGUPDATE_SUBCMD);
	msleep(5);

	while (i < CFG_UPDATE_POLLING_RETRY_LIMIT) {
		i++;
		flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, false);
		if (flags & (1 << 4))
			break;
		msleep(100);
	}

	if (i == CFG_UPDATE_POLLING_RETRY_LIMIT) {
		dev_err(di->dev, "%s: failed %04x\n", __func__, flags);
		return 0;
	}

	return 1;
}

static int exit_cfg_update_mode(struct bq27x00_device_info *di)
{
	int i = 0;
	u16 flags;

	dev_dbg(di->dev, "%s:\n", __func__);

	control_cmd_wr(di, BQ27441_SOFT_RESET);

	while (i < CFG_UPDATE_POLLING_RETRY_LIMIT) {
		i++;
		flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, false);
		if (!(flags & (1 << 4)))
			break;
		msleep(100);
	}

	if (i == CFG_UPDATE_POLLING_RETRY_LIMIT) {
		dev_err(di->dev, "%s: failed %04x\n", __func__, flags);
		return 0;
	}

	if (seal(di))
		return 1;
	else
		return 0;
}
static u8 checksum(u8 *data)
{
	u16 sum = 0;
	int i;

	for (i = 0; i < 32; i++)
		sum += data[i];

	sum &= 0xFF;

	return 0xFF - sum;
}

#ifdef DEBUG
static void print_buf(const char *msg, u8 *buf)
{
	int i;

	printk("\nbq: %s buf: ", msg);
	for (i = 0; i < 32; i++)
		printk("%02x ", buf[i]);

	printk("\n");
}
#else
#define print_buf(a, b)
#endif

static int update_dm_block(struct bq27x00_device_info *di, u8 subclass,
	u8 offset, u8 *data)
{
	u8 buf[32];
	u8 cksum;
	u8 blk_offset = offset >> 5;

	dev_dbg(di->dev, "%s: subclass %d offset %d\n",
		__func__, subclass, offset);

	di->bus.write(di, BLOCK_DATA_CONTROL, 0, true);
	msleep(5);

	di->bus.write(di, BLOCK_DATA_CLASS, subclass, true);
	msleep(5);

	di->bus.write(di, DATA_BLOCK, blk_offset, true);
	msleep(5);

	di->bus.blk_write(di, BLOCK_DATA, data, 32);
	msleep(5);
	print_buf(__func__, data);

	cksum = checksum(data);
	di->bus.write(di, BLOCK_DATA_CHECKSUM, cksum, true);
	msleep(5);

	/* Read back and compare to make sure write is successful */
	di->bus.write(di, DATA_BLOCK, blk_offset, true);
	msleep(5);
	di->bus.blk_read(di, BLOCK_DATA, buf, 32);
	if (memcmp(data, buf, 32)) {
		dev_err(di->dev, "%s: error updating subclass %d offset %d\n",
			__func__, subclass, offset);
		return 0;
	} else {
		return 1;
	}
}

static int read_dm_block(struct bq27x00_device_info *di, u8 subclass,
	u8 offset, u8 *data)
{
	u8 cksum_calc, cksum;
	u8 blk_offset = offset >> 5;

	dev_dbg(di->dev, "%s: subclass %d offset %d\n",
		__func__, subclass, offset);

	di->bus.write(di, BLOCK_DATA_CONTROL, 0, true);
	msleep(5);

	di->bus.write(di, BLOCK_DATA_CLASS, subclass, true);
	msleep(5);

	di->bus.write(di, DATA_BLOCK, blk_offset, true);
	msleep(5);

	di->bus.blk_read(di, BLOCK_DATA, data, 32);

	cksum_calc = checksum(data);
	cksum = di->bus.read(di, BLOCK_DATA_CHECKSUM, true);
	if (cksum != cksum_calc) {
		dev_err(di->dev, "%s: error reading subclass %d offset %d\n",
			__func__, subclass, offset);
		return 0;
	}

	print_buf(__func__, data);

	return 1;
}

/*
 * Return the battery State-of-Charge
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_soc(struct bq27x00_device_info *di)
{
	int soc;

	soc = bq27xxx_read(di, BQ27XXX_REG_SOC, false);

	if (soc < 0)
		dev_dbg(di->dev, "error reading relative State-of-Charge\n");

	return soc;
}

/*
 * Return a battery charge value in μAh
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_charge(struct bq27x00_device_info *di, u8 reg)
{
	int charge;

	charge = bq27xxx_read(di, reg, false);
	if (charge < 0) {
		dev_dbg(di->dev, "error reading charge register %02x: %d\n",
			reg, charge);
		return charge;
	}

	if (di->chip == BQ27200)
		charge = charge * 3570 / BQ27200_RS;
	else
		charge *= 1000;

	return charge;
}

/*
 * Return the battery Nominal available capaciy in μAh
 * Or < 0 if something fails.
 */
static inline int bq27x00_battery_read_nac(struct bq27x00_device_info *di)
{
	int flags;

	if (di->chip == BQ27200) {
		flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, true);
		if (flags >= 0 && (flags & BQ27200_FLAG_CI))
			return -ENODATA;
	}

	return bq27x00_battery_read_charge(di, BQ27XXX_REG_NAC);
}

/*
 * Return the battery Last measured discharge in μAh
 * Or < 0 if something fails.
 */
static inline int bq27x00_battery_read_fcc(struct bq27x00_device_info *di)
{
	return bq27x00_battery_read_charge(di, BQ27XXX_REG_FCC);
}

/*
 * Return the Design Capacity in μAh
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_dcap(struct bq27x00_device_info *di)
{
	int dcap;

	dcap = bq27xxx_read(di, BQ27XXX_REG_DCAP, false);

	if (dcap < 0) {
		dev_dbg(di->dev, "error reading initial last measured discharge\n");
		return dcap;
	}

	if (di->chip == BQ27200)
		dcap = dcap * 256 * 3570 / BQ27200_RS;
	else
		dcap *= 1000;

	return dcap;
}

/*
 * Return the battery Available energy in μWh
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_energy(struct bq27x00_device_info *di)
{
	int ae;

	ae = bq27xxx_read(di, BQ27XXX_REG_AE, false);
	if (ae < 0) {
		dev_dbg(di->dev, "error reading available energy\n");
		return ae;
	}

	if (di->chip == BQ27200)
		ae = ae * 29200 / BQ27200_RS;
	else
		ae *= 1000;

	return ae;
}

/*
 * Return the battery temperature in tenths of degree Kelvin
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_temperature(struct bq27x00_device_info *di)
{
	int temp;

	temp = bq27xxx_read(di, BQ27XXX_REG_TEMP, false);
	if (temp < 0) {
		dev_err(di->dev, "error reading temperature\n");
		return temp;
	}

	if (di->chip == BQ27200)
		temp = 5 * temp / 2;

	return temp;
}

/*
 * Return the battery Cycle count total
 * Or < 0 if something fails.
 */
static int bq27x00_battery_read_cyct(struct bq27x00_device_info *di)
{
	int cyct;

	cyct = bq27xxx_read(di, BQ27XXX_REG_CYCT, false);
	if (cyct < 0)
		dev_err(di->dev, "error reading cycle count total\n");

	return cyct;
}

/*
 * Read a time register.
 * Return < 0 if something fails.
 */
static int bq27x00_battery_read_time(struct bq27x00_device_info *di, u8 reg)
{
	int tval;

	tval = bq27xxx_read(di, reg, false);
	if (tval < 0) {
		dev_dbg(di->dev, "error reading time register %02x: %d\n",
			reg, tval);
		return tval;
	}

	if (tval == 65535)
		return -ENODATA;

	return tval * 60;
}

/*
 * Read a power avg register.
 * Return < 0 if something fails.
 */
static int bq27x00_battery_read_pwr_avg(struct bq27x00_device_info *di, u8 reg)
{
	int tval;

	tval = bq27xxx_read(di, reg, false);
	if (tval < 0) {
		dev_err(di->dev, "error reading power avg rgister  %02x: %d\n",
			reg, tval);
		return tval;
	}

	if (di->chip == BQ27200)
		return (tval * BQ27200_POWER_CONSTANT) / BQ27200_RS;
	else
		return tval;
}

static int overtemperature(struct bq27x00_device_info *di, u16 flags)
{
	if (di->chip == BQ27520)
		return flags & (BQ27XXX_FLAG_OTC | BQ27XXX_FLAG_OTD);
	else
		return flags & BQ27XXX_FLAG_OTC;
}

/*
 * Read flag register.
 * Return < 0 if something fails.
 */
static int bq27x00_battery_read_health(struct bq27x00_device_info *di)
{
	u16 tval;

	tval = bq27xxx_read(di, BQ27XXX_REG_FLAGS, false);
	if (tval < 0) {
		dev_err(di->dev, "error reading flag register:%d\n", tval);
		return tval;
	}

	if ((di->chip == BQ27200)) {
		if (tval & BQ27200_FLAG_EDV1)
			tval = POWER_SUPPLY_HEALTH_DEAD;
		else
			tval = POWER_SUPPLY_HEALTH_GOOD;
		return tval;
	} else {
		if (tval & BQ27XXX_FLAG_SOCF)
			tval = POWER_SUPPLY_HEALTH_DEAD;
		else if (overtemperature(di, tval))
			tval = POWER_SUPPLY_HEALTH_OVERHEAT;
		else
			tval = POWER_SUPPLY_HEALTH_GOOD;
		return tval;
	}

	return -1;
}

static void bq27x00_update(struct bq27x00_device_info *di)
{
	struct bq27x00_reg_cache cache = {0, };
	bool is_bq27200 = di->chip == BQ27200;
	bool is_bq27500 = di->chip == BQ27500;
	bool is_bq27441 = di->chip == BQ27441;
	bool is_bq276xx = di->chip == BQ276XX;

	cache.flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, !is_bq27500);
	if (cache.flags >= 0) {
		if (is_bq27200 && (cache.flags & BQ27200_FLAG_CI)) {
			cache.capacity = -ENODATA;
			cache.energy = -ENODATA;
			cache.time_to_empty = -ENODATA;
			cache.time_to_empty_avg = -ENODATA;
			cache.time_to_full = -ENODATA;
			cache.charge_full = -ENODATA;
			cache.health = -ENODATA;
		} else {
			cache.capacity = bq27x00_battery_read_soc(di);
			g_capacity = cache.capacity;
			if (!(is_bq27441 || is_bq276xx)) {
				cache.energy = bq27x00_battery_read_energy(di);
				cache.time_to_empty =
					bq27x00_battery_read_time(di,
							BQ27XXX_REG_TTE);
				cache.time_to_empty_avg =
					bq27x00_battery_read_time(di,
							BQ27XXX_REG_TTECP);
				cache.time_to_full =
					bq27x00_battery_read_time(di,
							BQ27XXX_REG_TTF);
			}
			cache.charge_full = bq27x00_battery_read_fcc(di);
			cache.health = bq27x00_battery_read_health(di);
		}
		cache.temperature = bq27x00_battery_read_temperature(di);
		if (!is_bq27441)
			cache.cycle_count = bq27x00_battery_read_cyct(di);
		cache.power_avg =
			bq27x00_battery_read_pwr_avg(di, BQ27XXX_POWER_AVG);

		/* We only have to read charge design full once */
		if ((di->charge_design_full <= 0) || por_detect_flag) {
			di->charge_design_full = bq27x00_battery_read_dcap(di);
		}	
	}

	if (memcmp(&di->cache, &cache, sizeof(cache)) != 0) {
		di->cache = cache;
		power_supply_changed(&di->bat);
	}

	di->last_update = jiffies;
}

static void copy_to_dm_buf_big_endian(struct bq27x00_device_info *di,
	u8 *buf, u8 offset, u8 sz, u32 val)
{
	dev_dbg(di->dev, "%s: offset %d sz %d val %d\n",
		__func__, offset, sz, val);

	switch (sz) {
	case 1:
		buf[offset] = (u8) val;
		break;
	case 2:
		put_unaligned_be16((u16) val, &buf[offset]);
		break;
	case 4:
		put_unaligned_be32(val, &buf[offset]);
		break;
	default:
		dev_err(di->dev, "%s: bad size for dm parameter - %d",
			__func__, sz);
		break;
	}
}

static int rom_mode_gauge_init_completed(struct bq27x00_device_info *di)
{
	dev_dbg(di->dev, "%s:\n", __func__);

	return control_cmd_read(di, CONTROL_STATUS_SUBCMD) &
		BQ27441_CTRL_STATUS_INITCOMP;
}

static bool rom_mode_gauge_dm_initialized(struct bq27x00_device_info *di)
{
	u16 flags;

	flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, false);

	dev_dbg(di->dev, "%s: flags - 0x%04x\n", __func__, flags);

	if (flags & BQ27441_FLAG_ITPOR)
		return false;
	else
		return true;
}

#define INITCOMP_TIMEOUT_MS		10000
static void rom_mode_gauge_dm_init(struct bq27x00_device_info *di)
{
	int i;
	int timeout = INITCOMP_TIMEOUT_MS;
	u8 subclass, offset;
	u32 blk_number;
	u32 blk_number_prev = 0;
	u8 buf[32];
	bool buf_valid = false;
	struct dm_reg *dm_reg;

	dev_dbg(di->dev, "%s:\n", __func__);

	while (!rom_mode_gauge_init_completed(di) && timeout > 0) {
		msleep(100);
		timeout -= 100;
	}

	if (timeout <= 0) {
		dev_err(di->dev, "%s: INITCOMP not set after %d seconds\n",
			__func__, INITCOMP_TIMEOUT_MS/100);
		return;
	}

	if (!di->dm_regs || !di->dm_regs_count) {
		dev_err(di->dev, "%s: Data not available for DM initialization\n",
			__func__);
		return;
	}

	enter_cfg_update_mode(di);
	for (i = 0; i < di->dm_regs_count; i++) {
		dm_reg = &di->dm_regs[i];
		subclass = dm_reg->subclass;
		offset = dm_reg->offset;

		/*
		 * Create a composite block number to see if the subsequent
		 * register also belongs to the same 32 btye block in the DM
		 */
		blk_number = subclass << 8;
		blk_number |= offset >> 5;

		if (blk_number == blk_number_prev) {
			copy_to_dm_buf_big_endian(di, buf, offset,
				dm_reg->len, dm_reg->data);
		} else {

			if (buf_valid)
				update_dm_block(di, blk_number_prev >> 8,
					(blk_number_prev << 5) & 0xFF , buf);
			else
				buf_valid = true;

			read_dm_block(di, dm_reg->subclass, dm_reg->offset,
				buf);
			copy_to_dm_buf_big_endian(di, buf, offset,
				dm_reg->len, dm_reg->data);
		}
		blk_number_prev = blk_number;
	}

	/* Last buffer to be written */
	if (buf_valid)
		update_dm_block(di, subclass, offset, buf);

	exit_cfg_update_mode(di);
}

static void bq27x00_battery_poll(struct work_struct *work)
{
	struct bq27x00_device_info *di =
		container_of(work, struct bq27x00_device_info, work.work);

	if (((di->chip == BQ27441) || (di->chip == BQ276XX)) &&
		!rom_mode_gauge_dm_initialized(di)) {
		por_detect_flag = 1;
		rom_mode_gauge_dm_init(di);
	}

	bq27x00_update(di);

	if (poll_interval > 0) {
		/* The timer does not have to be accurate. */
		set_timer_slack(&di->work.timer, poll_interval * HZ / 4);
		schedule_delayed_work(&di->work, poll_interval * HZ);
	}
}

/*
 * Return the battery average current in μA
 * Note that current can be negative signed as well
 * Or 0 if something fails.
 */
static int bq27x00_battery_current(struct bq27x00_device_info *di,
	union power_supply_propval *val)
{
	int curr;
	int flags;

	curr = bq27xxx_read(di, BQ27XXX_REG_AI, false);
	if (curr < 0) {
		dev_err(di->dev, "error reading current\n");
		return curr;
	}

	if (di->chip == BQ27200) {
		flags = bq27xxx_read(di, BQ27XXX_REG_FLAGS, false);
		if (flags & BQ27200_FLAG_CHGS) {
			dev_dbg(di->dev, "negative current!\n");
			curr = -curr;
		}

		val->intval = curr * 3570 / BQ27200_RS;
	} else {
		/* Other gauges return signed value */
		val->intval = (int)((s16)curr) * 1000;
	}

	return 0;
}

static int bq27x00_battery_status(struct bq27x00_device_info *di,
	union power_supply_propval *val)
{
	int status;

	if (di->chip == BQ27200) {
		if (di->cache.flags & BQ27200_FLAG_FC)
			status = POWER_SUPPLY_STATUS_FULL;
		else if (di->cache.flags & BQ27200_FLAG_CHGS)
			status = POWER_SUPPLY_STATUS_CHARGING;
		else if (power_supply_am_i_supplied(&di->bat))
			status = POWER_SUPPLY_STATUS_NOT_CHARGING;
		else
			status = POWER_SUPPLY_STATUS_DISCHARGING;
	} else {
		
		if (di->cache.flags & BQ27XXX_FLAG_FC) {
			status = POWER_SUPPLY_STATUS_FULL;}
		else if (di->cache.flags & BQ27XXX_FLAG_DSC) { 
			status = POWER_SUPPLY_STATUS_DISCHARGING;}
		else {
			status = POWER_SUPPLY_STATUS_CHARGING;}
	}

	val->intval = status;

	return 0;
}

static int bq27x00_battery_capacity_level(struct bq27x00_device_info *di,
	union power_supply_propval *val)
{
	int level;
	
	if (di->chip == BQ27200) {
		if (di->cache.flags & BQ27200_FLAG_FC)
			level = POWER_SUPPLY_CAPACITY_LEVEL_FULL;
		else if (di->cache.flags & BQ27200_FLAG_EDV1)
			level = POWER_SUPPLY_CAPACITY_LEVEL_LOW;
		else if (di->cache.flags & BQ27200_FLAG_EDVF)
			level = POWER_SUPPLY_CAPACITY_LEVEL_CRITICAL;
		else
			level = POWER_SUPPLY_CAPACITY_LEVEL_NORMAL;
	} else {
		if (di->cache.flags & BQ27XXX_FLAG_FC) {
			level = POWER_SUPPLY_CAPACITY_LEVEL_FULL;}
		else if (di->cache.flags & BQ27XXX_FLAG_SOC1) {
			level = POWER_SUPPLY_CAPACITY_LEVEL_LOW;}
		else if (di->cache.flags & BQ27XXX_FLAG_SOCF) {
			level = POWER_SUPPLY_CAPACITY_LEVEL_CRITICAL;}
		else {
			level = POWER_SUPPLY_CAPACITY_LEVEL_NORMAL;}
	}

	val->intval = level;

	return 0;
}

/*
 * Return the battery Voltage in millivolts
 * Or < 0 if something fails.
 */
int voltage = 0;

static int bq27x00_battery_voltage(struct bq27x00_device_info *di,
	union power_supply_propval *val)
{
	int volt;
	
	/*gpio_direction_output(CHARGE_EN,1);
	gpio_set_value(CHARGE_EN,1);
	mdelay(20);*/
	volt = bq27xxx_read(di, BQ27XXX_REG_VOLT, false);
	//gpio_set_value(CHARGE_EN,0);

	if (volt < 0) {
		dev_err(di->dev, "error reading voltage\n");
		return volt;
	}

	voltage = volt;
	val->intval = volt * 1000;

	return 0;
}

u32 bq27441_battery_voltage(void)
{
	int bq27441_volt;

	bq27441_volt = voltage;

	return bq27441_volt;
}
EXPORT_SYMBOL_GPL(bq27441_battery_voltage);

static int bq27x00_simple_value(int value,
	union power_supply_propval *val)
{
	if (value < 0)
		return value;

	val->intval = value;

	return 0;
}

#define to_bq27x00_device_info(x) container_of((x), \
				struct bq27x00_device_info, bat);

static int bq27x00_battery_get_property(struct power_supply *psy,
					enum power_supply_property psp,
					union power_supply_propval *val)
{
	int ret = 0;
	struct bq27x00_device_info *di = to_bq27x00_device_info(psy);

	mutex_lock(&di->lock);
	if (time_is_before_jiffies(di->last_update + 5 * HZ)) {
		cancel_delayed_work_sync(&di->work);
		bq27x00_battery_poll(&di->work.work);
	}
	mutex_unlock(&di->lock);

	if (psp != POWER_SUPPLY_PROP_PRESENT && di->cache.flags < 0)
		return -ENODEV;

	switch (psp) {
	case POWER_SUPPLY_PROP_STATUS:
		ret = bq27x00_battery_status(di, val);
		break;
	case POWER_SUPPLY_PROP_VOLTAGE_NOW:
		ret = bq27x00_battery_voltage(di, val);
		bq27441_battery_voltage();
		break;
	case POWER_SUPPLY_PROP_PRESENT:
		val->intval = di->cache.flags < 0 ? 0 : 1;
		break;
	case POWER_SUPPLY_PROP_CURRENT_NOW:
		ret = bq27x00_battery_current(di, val);
		break;
	case POWER_SUPPLY_PROP_CAPACITY:
		ret = bq27x00_simple_value(di->cache.capacity, val);
		break;
	case POWER_SUPPLY_PROP_CAPACITY_LEVEL:
		ret = bq27x00_battery_capacity_level(di, val);
		break;
	case POWER_SUPPLY_PROP_TEMP:
		ret = bq27x00_simple_value(di->cache.temperature, val);
		if (ret == 0)
			val->intval -= 2731;
		break;
	case POWER_SUPPLY_PROP_TIME_TO_EMPTY_NOW:
		ret = bq27x00_simple_value(di->cache.time_to_empty, val);
		break;
	case POWER_SUPPLY_PROP_TIME_TO_EMPTY_AVG:
		ret = bq27x00_simple_value(di->cache.time_to_empty_avg, val);
		break;
	case POWER_SUPPLY_PROP_TIME_TO_FULL_NOW:
		ret = bq27x00_simple_value(di->cache.time_to_full, val);
		break;
	case POWER_SUPPLY_PROP_TECHNOLOGY:
		val->intval = POWER_SUPPLY_TECHNOLOGY_LION;
		break;
	case POWER_SUPPLY_PROP_CHARGE_NOW:
		ret = bq27x00_simple_value(bq27x00_battery_read_nac(di), val);
		break;
	case POWER_SUPPLY_PROP_CHARGE_FULL:
		ret = bq27x00_simple_value(di->cache.charge_full, val);
		break;
	case POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN:
		ret = bq27x00_simple_value(di->charge_design_full, val);
		break;
	case POWER_SUPPLY_PROP_CYCLE_COUNT:
		ret = bq27x00_simple_value(di->cache.cycle_count, val);
		break;
	case POWER_SUPPLY_PROP_ENERGY_NOW:
		ret = bq27x00_simple_value(di->cache.energy, val);
		break;
	case POWER_SUPPLY_PROP_POWER_AVG:
		ret = bq27x00_simple_value(di->cache.power_avg, val);
		break;
	case POWER_SUPPLY_PROP_HEALTH:
		ret = bq27x00_simple_value(di->cache.health, val);
		break;
	default:
		return -EINVAL;
	}

	return ret;
}

static void bq27x00_external_power_changed(struct power_supply *psy)
{
	struct bq27x00_device_info *di = to_bq27x00_device_info(psy);

	cancel_delayed_work_sync(&di->work);
	schedule_delayed_work(&di->work, 0);
}

static void __init set_properties_array(struct bq27x00_device_info *di,
	enum power_supply_property *props, int num_props)
{
	int tot_sz = num_props * sizeof(enum power_supply_property);

	di->bat.properties = devm_kzalloc(di->dev, tot_sz, GFP_KERNEL);

	if (di->bat.properties) {
		memcpy(di->bat.properties, props, tot_sz);
		di->bat.num_properties = num_props;
	} else {
		di->bat.num_properties = 0;
	}
}

static int __init bq27x00_powersupply_init(struct bq27x00_device_info *di)
{
	int ret;

	di->bat.type = POWER_SUPPLY_TYPE_BATTERY;
	if (di->chip == BQ27441) {
		set_properties_array(di, bq27441_battery_props,
			ARRAY_SIZE(bq27441_battery_props));
	} else if (di->chip == BQ276XX) {
		set_properties_array(di, bq276xx_battery_props,
			ARRAY_SIZE(bq276xx_battery_props));
	} else if (di->chip == BQ27520) {
		set_properties_array(di, bq27520_battery_props,
			ARRAY_SIZE(bq27520_battery_props));
	} else if (di->chip == BQ2753X) {
		set_properties_array(di, bq2753x_battery_props,
			ARRAY_SIZE(bq2753x_battery_props));
	} else {
		set_properties_array(di, bq27x00_battery_props,
			ARRAY_SIZE(bq27x00_battery_props));
	}
	di->bat.get_property = bq27x00_battery_get_property;
	di->bat.external_power_changed = bq27x00_external_power_changed;

	INIT_DELAYED_WORK(&di->work, bq27x00_battery_poll);
	mutex_init(&di->lock);

	ret = power_supply_register(di->dev, &di->bat);
	if (ret) {
		dev_err(di->dev, "failed to register battery: %d\n", ret);
		return ret;
	}

	dev_info(di->dev, "support ver. %s enabled\n", DRIVER_VERSION);

	bq27x00_update(di);

	return 0;
}

static void bq27x00_powersupply_unregister(struct bq27x00_device_info *di)
{
	/*
	 * power_supply_unregister call bq27x00_battery_get_property which
	 * call bq27x00_battery_poll.
	 * Make sure that bq27x00_battery_poll will not call
	 * schedule_delayed_work again after unregister (which cause OOPS).
	 */
	poll_interval = 0;

	cancel_delayed_work_sync(&di->work);

	power_supply_unregister(&di->bat);

	mutex_destroy(&di->lock);
}


/* i2c specific code */
#ifdef CONFIG_BATTERY_BQ27441_I2C

/* If the system has several batteries we need a different name for each
 * of them...
 */
static DEFINE_IDR(battery_id);
static DEFINE_MUTEX(battery_mutex);

static int bq27xxx_read_i2c(struct bq27x00_device_info *di, u8 reg, bool single)
{
	struct i2c_client *client = to_i2c_client(di->dev);
	struct i2c_msg msg[2];
	unsigned char data[2];
	int ret;

	if (!client->adapter)
		return -ENODEV;

	msg[0].addr = client->addr;
	msg[0].flags = 0;
	msg[0].buf = &reg;
	msg[0].len = sizeof(reg);
	msg[1].addr = client->addr;
	msg[1].flags = I2C_M_RD;
	msg[1].buf = data;
	if (single)
		msg[1].len = 1;
	else
		msg[1].len = 2;

	ret = i2c_transfer(client->adapter, msg, ARRAY_SIZE(msg));
	if (ret < 0)
		return ret;

	if (!single)
		ret = get_unaligned_le16(data);
	else
		ret = data[0];

	return ret;
}

static int bq27xxx_write_i2c(struct bq27x00_device_info *di, u8 reg, int value, bool single)
{
	struct i2c_client *client = to_i2c_client(di->dev);
	struct i2c_msg msg;
	unsigned char data[4];
	int ret;

	if (!client->adapter)
		return -ENODEV;

	data[0] = reg;
	if (single) {
		data[1] = (unsigned char)value;
		msg.len = 2;
	} else {
		put_unaligned_le16(value, &data[1]);
		msg.len = 3;
	}

	msg.buf = data;
	msg.addr = client->addr;
	msg.flags = 0;

	ret = i2c_transfer(client->adapter, &msg, 1);
	if (ret < 0)
		return ret;

	return 0;
}

static int bq27xxx_read_i2c_blk(struct bq27x00_device_info *di, u8 reg,
	u8 *data, u8 len)
{
	struct i2c_client *client = to_i2c_client(di->dev);
	struct i2c_msg msg[2];
	int ret;

	if (!client->adapter)
		return -ENODEV;

	msg[0].addr = client->addr;
	msg[0].flags = 0;
	msg[0].buf = &reg;
	msg[0].len = 1;

	msg[1].addr = client->addr;
	msg[1].flags = I2C_M_RD;
	msg[1].buf = data;
	msg[1].len = len;

	ret = i2c_transfer(client->adapter, msg, ARRAY_SIZE(msg));
	if (ret < 0)
		return ret;

	return ret;
}

static int bq27xxx_write_i2c_blk(struct bq27x00_device_info *di, u8 reg,
	u8 *data, u8 sz)
{
	struct i2c_client *client = to_i2c_client(di->dev);
	struct i2c_msg msg;
	int ret;
	u8 buf[33];

	if (!client->adapter)
		return -ENODEV;

	buf[0] = reg;
	memcpy(&buf[1], data, sz);

	msg.buf = buf;
	msg.addr = client->addr;
	msg.flags = 0;
	msg.len = sz + 1;

	ret = i2c_transfer(client->adapter, &msg, 1);
	if (ret < 0)
		return ret;

	return 0;
}

static int bq27x00_battery_reset(struct bq27x00_device_info *di)
{

	bq27xxx_write(di, BQ27XXX_REG_CTRL, RESET_SUBCMD, false);

	msleep(10);

	return bq27xxx_read(di, BQ27XXX_REG_CTRL, false);
}

static int bq27x00_battery_read_fw_version(struct bq27x00_device_info *di)
{
	bq27xxx_write(di, BQ27XXX_REG_CTRL, FW_VER_SUBCMD, false);

	msleep(10);

	return bq27xxx_read(di, BQ27XXX_REG_CTRL, false);
}

static int bq27x00_battery_read_device_type(struct bq27x00_device_info *di)
{
	bq27xxx_write(di, BQ27XXX_REG_CTRL, DEV_TYPE_SUBCMD, false);

	msleep(10);

	return bq27xxx_read(di, BQ27XXX_REG_CTRL, false);
}

static int bq27x00_battery_read_dataflash_version(struct bq27x00_device_info *di)
{
	bq27xxx_write(di, BQ27XXX_REG_CTRL, DF_VER_SUBCMD, false);

	msleep(10);

	return bq27xxx_read(di, BQ27XXX_REG_CTRL, false);
}

static ssize_t show_firmware_version(struct device *dev,
		struct device_attribute *attr, char *buf)
{
	struct bq27x00_device_info *di = dev_get_drvdata(dev);
	int ver;

	ver = bq27x00_battery_read_fw_version(di);

	return sprintf(buf, "%d\n", ver);
}

static ssize_t show_dataflash_version(struct device *dev,
		struct device_attribute *attr, char *buf)
{
	struct bq27x00_device_info *di = dev_get_drvdata(dev);
	int ver;

	ver = bq27x00_battery_read_dataflash_version(di);

	return sprintf(buf, "%d\n", ver);
}

static ssize_t show_device_type(struct device *dev,
		struct device_attribute *attr, char *buf)
{
	struct bq27x00_device_info *di = dev_get_drvdata(dev);
	int dev_type;

	dev_type = bq27x00_battery_read_device_type(di);

	return sprintf(buf, "%d\n", dev_type);
}

static ssize_t show_reset(struct device *dev,
		struct device_attribute *attr, char *buf)
{
	struct bq27x00_device_info *di = dev_get_drvdata(dev);

	bq27x00_battery_reset(di);

	return sprintf(buf, "okay\n");
}


static ssize_t show_por_detect(struct device *dev,
			    struct device_attribute *attr, char *buf)
{
	return sprintf(buf, "OK\n");
}

static ssize_t store_por_detect(struct device *dev,
			     struct device_attribute *attr, const char *buf,
			     size_t count)
{
	int ret;
	unsigned long data;
	struct bq27x00_device_info *di = dev_get_drvdata(dev);

	ret = strict_strtoul(buf, 10, &data);
	if(data) {
		printk("bq27441 update charge_full_design\n");
		di->charge_design_full = bq27x00_battery_read_dcap(di);
	}
	else {
		printk("bq27441 disable update charge_full_design\n");
		por_detect_flag = 0;
	}

	return count;
}



static DEVICE_ATTR(fw_version, S_IRUGO, show_firmware_version, NULL);
static DEVICE_ATTR(df_version, S_IRUGO, show_dataflash_version, NULL);
static DEVICE_ATTR(device_type, S_IRUGO, show_device_type, NULL);
static DEVICE_ATTR(reset, S_IRUGO, show_reset, NULL);
static DEVICE_ATTR(por_detect, S_IRUSR | S_IWUSR, show_por_detect, store_por_detect);


static struct attribute *bq27x00_attributes[] = {
	&dev_attr_fw_version.attr,
	&dev_attr_df_version.attr,
	&dev_attr_device_type.attr,
	&dev_attr_reset.attr,
	&dev_attr_por_detect.attr,
	NULL
};

static const struct attribute_group bq27x00_attr_group = {
	.attrs = bq27x00_attributes,
};

static int __init bq27x00_battery_probe(struct i2c_client *client,
				 const struct i2c_device_id *id)
{
	char *name;
	struct bq27x00_device_info *di;
	int num;
	int retval = 0;
	u8 *regs;

	/* Get new ID for the new battery device */
	retval = idr_pre_get(&battery_id, GFP_KERNEL);
	if (retval == 0)
		return -ENOMEM;
	mutex_lock(&battery_mutex);
	retval = idr_get_new(&battery_id, client, &num);
	mutex_unlock(&battery_mutex);
	if (retval < 0)
		return retval;

	name = kasprintf(GFP_KERNEL, "%s-%d", id->name, num);
	if (!name) {
		dev_err(&client->dev, "failed to allocate device name\n");
		retval = -ENOMEM;
		goto batt_failed_1;
	}

	di = kzalloc(sizeof(*di), GFP_KERNEL);
	if (!di) {
		dev_err(&client->dev, "failed to allocate device info data\n");
		retval = -ENOMEM;
		goto batt_failed_2;
	}

	di->id = num;
	di->dev = &client->dev;
	di->chip = id->driver_data;
	di->bat.name = name;
	di->bus.read = &bq27xxx_read_i2c;
	di->bus.write = &bq27xxx_write_i2c;
	di->bus.blk_read = bq27xxx_read_i2c_blk;
	di->bus.blk_write = bq27xxx_write_i2c_blk;
	di->dm_regs = NULL;
	di->dm_regs_count = 0;

	if (di->chip == BQ27200)
		regs = bq27200_regs;
	else if (di->chip == BQ27500)
		regs = bq27500_regs;
	else if (di->chip == BQ27520)
		regs = bq27520_regs;
	else if (di->chip == BQ2753X)
		regs = bq2753x_regs;
	else if (di->chip == BQ27441) {
		regs = bq27441_regs;
		di->dm_regs = bq27441_dm_regs;
		di->dm_regs_count = ARRAY_SIZE(bq27441_dm_regs);
	} else if (di->chip == BQ276XX) {
		/* commands are same as bq274xx, only DM is different */
		regs = bq276xx_regs;
		di->dm_regs = bq276xx_dm_regs;
		di->dm_regs_count = ARRAY_SIZE(bq276xx_dm_regs);
	} else {
		dev_err(&client->dev,
			"Unexpected gas gague: %d\n", di->chip);
		regs = bq27520_regs;
	}

	memcpy(di->regs, regs, NUM_REGS);

	di->fw_ver = bq27x00_battery_read_fw_version(di);

	retval = bq27x00_powersupply_init(di);
	if (retval)
		goto batt_failed_3;

	/* Schedule a polling after about 1 min */
	schedule_delayed_work(&di->work, 60 * HZ);

	i2c_set_clientdata(client, di);
	retval = sysfs_create_group(&client->dev.kobj, &bq27x00_attr_group);
	if (retval)
		dev_err(&client->dev, "could not create sysfs files\n");

	return 0;

batt_failed_3:
	kfree(di);
batt_failed_2:
	kfree(name);
batt_failed_1:
	mutex_lock(&battery_mutex);
	idr_remove(&battery_id, num);
	mutex_unlock(&battery_mutex);

	return retval;
}

static int bq27x00_battery_remove(struct i2c_client *client)
{
	struct bq27x00_device_info *di = i2c_get_clientdata(client);

	bq27x00_powersupply_unregister(di);

	kfree(di->bat.name);

	mutex_lock(&battery_mutex);
	idr_remove(&battery_id, di->id);
	mutex_unlock(&battery_mutex);

	kfree(di);

	return 0;
}

static const struct i2c_device_id bq27x00_id[] = {
	{ "bq27200", BQ27200 },
	{ "bq27500", BQ27500 },
	{ "bq27520", BQ27520 },
	{ "bq27441", BQ27441 },
	{ "bq276xx", BQ276XX },
	{ "bq2753x", BQ2753X },
	{},
};
MODULE_DEVICE_TABLE(i2c, bq27x00_id);

static struct i2c_driver bq27x00_battery_driver = {
	.driver = {
		.name = "bq27441",
	},
	.probe = bq27x00_battery_probe,
	.remove = bq27x00_battery_remove,
	.id_table = bq27x00_id,
};

module_i2c_driver(bq27x00_battery_driver);

#endif

/* platform specific code */
#ifdef CONFIG_BATTERY_BQ27441_PLATFORM

static int bq27000_read_platform(struct bq27x00_device_info *di, u8 reg,
			bool single)
{
	struct device *dev = di->dev;
	struct bq27000_platform_data *pdata = dev->platform_data;
	unsigned int timeout = 3;
	int upper, lower;
	int temp;

	if (!single) {
		/* Make sure the value has not changed in between reading the
		 * lower and the upper part */
		upper = pdata->read(dev, reg + 1);
		do {
			temp = upper;
			if (upper < 0)
				return upper;

			lower = pdata->read(dev, reg);
			if (lower < 0)
				return lower;

			upper = pdata->read(dev, reg + 1);
		} while (temp != upper && --timeout);

		if (timeout == 0)
			return -EIO;

		return (upper << 8) | lower;
	}

	return pdata->read(dev, reg);
}

static int bq27000_battery_probe(struct platform_device *pdev)
{
	struct bq27x00_device_info *di;
	struct bq27000_platform_data *pdata = pdev->dev.platform_data;
	int ret;

	if (!pdata) {
		dev_err(&pdev->dev, "no platform_data supplied\n");
		return -EINVAL;
	}

	if (!pdata->read) {
		dev_err(&pdev->dev, "no hdq read callback supplied\n");
		return -EINVAL;
	}

	di = kzalloc(sizeof(*di), GFP_KERNEL);
	if (!di) {
		dev_err(&pdev->dev, "failed to allocate device info data\n");
		return -ENOMEM;
	}

	platform_set_drvdata(pdev, di);

	di->dev = &pdev->dev;
	di->chip = BQ27200;

	di->bat.name = pdata->name ?: dev_name(&pdev->dev);
	di->bus.read = &bq27000_read_platform;

	ret = bq27x00_powersupply_init(di);
	if (ret)
		goto err_free;

	return 0;

err_free:
	kfree(di);

	return ret;
}

static int bq27000_battery_remove(struct platform_device *pdev)
{
	struct bq27x00_device_info *di = platform_get_drvdata(pdev);

	bq27x00_powersupply_unregister(di);

	kfree(di);

	return 0;
}

static struct platform_driver __initdata bq27000_battery_driver = {
	.probe	= bq27000_battery_probe,
	.remove = bq27000_battery_remove,
	.driver = {
		.name = "bq27000-battery",
		.owner = THIS_MODULE,
	},
};

static inline int bq27x00_battery_platform_init(void)
{
	int ret = platform_driver_register(&bq27000_battery_driver);
	if (ret)
		printk(KERN_ERR "Unable to register BQ27200 platform driver\n");

	return ret;
}

static inline void bq27x00_battery_platform_exit(void)
{
	platform_driver_unregister(&bq27000_battery_driver);
}

#else

static inline int bq27x00_battery_platform_init(void) { return 0; }
static inline void bq27x00_battery_platform_exit(void) {};

#endif

/*
 * Module stuff
 */

static int __init bq27x00_battery_init(void)
{
	int ret;

	ret = bq27x00_battery_platform_init();

	return ret;
}
module_init(bq27x00_battery_init);

static void __exit bq27x00_battery_exit(void)
{
	bq27x00_battery_platform_exit();
}
module_exit(bq27x00_battery_exit);

MODULE_AUTHOR("Rodolfo Giometti <giometti@linux.it>");
MODULE_DESCRIPTION("BQ27x00 battery monitor driver");
MODULE_LICENSE("GPL");

The I2C communication is normal and the register values, including fw_version, can be read correctly. But the bit INITCOMP is always 0.

ITPOR is 1, and then polls to read the CONTROL_STATUS[INITCOMP] bit. It polls for a long time, many times, and it is still 0.

Waiting for your reply.

Thanks

Star