This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mosfet N breakdown

Part Number: LM5149-Q1


I describe the phenomenon I encountered:
 
- Input: 30V
- Output: 12V
When I don't load the output, everything works normally
After I tested the output capacity of 12V-3A, mosfet Q1 was broken, causing V-IN to connect to V-Out.
I will attach my design at the below.