hello:
The customer wants to know the voltage range of TPS612592YFFR during operation. The circuit diagram is shown below:
the current is about 1.5A,and it is used in PAD product,Thanks!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello:
The customer wants to know the voltage range of TPS612592YFFR during operation. The circuit diagram is shown below:
the current is about 1.5A,and it is used in PAD product,Thanks!!!
Hi Jimmy,
Do you mean the min VIN that can support 1.5A load current? It should be 3V. You can use power stage tool to double check this.
About the schematic, TPS612592 can't support 2 pcs 10uF/0402 at 1.5A load current, the effective capacitance should be within this range.
Please also refer to these notes in datasheet about COUT selection.
Regards,
Nathan