Part Number: TPS51396A
Hi,
I have a problem with the IC TPS51396A when I try to power on. After enable a sort circuit is created between VCC #17 with GND .
On my design I have 5 same IC TPS51396A. The problem is the sort circuit is happening only on two specific of them every time.
There are two ways to enable them.
- Either with 5V voltage rail, it is generated after Vin pgood.
- Or with external controller providing 3.3V
Both of them are failing.
Could you please provide insight about what could be the root cause?
Schematic & layout attached.

Layout
Thank in advance,